Hardware requirements
Micro USB cable
MC56F80000-EVK board
Personal Computer
Board hardware common setting
Power setting:
Connect J8 pin2 and pin3 Connect J6 pin1 and pin2 Connect J5 pin1 and pin2
Reset pin setting:
Connect J11 pin2 and pin3
Debugger setting:
Connect J13 pin 1-2, 3-4, 5-6, 7-8
Board settings
No special settings are required.
Note: The sample0 works in fully differential mode and the differential pair is selected as ANA6 and ANA7. And the thermistor in MC56F80000-EVK board is connected to ANA6 and ANA7.
Prepare the Demo
Connect USB cable between the host PC and the J12 USB port on the target board. It setups Multilink and COM port in PC device manager.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board with Multilink debug configuration.
Launch the debugger in your IDE to begin running the demo.
Running the demo
When the example runs successfully, wait 2 seconds for the ADC conversion result to refresh once. The terminal displays the following information:
CADC PIT trigger EDMA conversion.
ADC value: 3122
ADC value: 3122
ADC value: 3122
ADC value: 3122
ADC value: 3122
ADC value: 3122
ADC value: 3122
ADC value: 3122
ADC value: 3122
ADC value: 3122
The ADC input channel is connected with thermistor,so touching thermistor on board will get the ADC value updated.