Hardware requirements

  • USB Type-C cable

  • MCIMX93AUTO-EVK board

  • J-Link Debug Probe

  • 12V~20V power supply

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo

  1. Connect 12V~20V power supply and J-Link Debug Probe to the board, switch SW2 to power on the board.

  2. Connect a USB Type-C cable between the host PC and the J26 USB port on the target board.

  3. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  4. Download the program to the target board.

  5. Either re-power up your board or launch the debugger in your IDE to begin running the example.

Running the demo

When the example runs successfully, you can see the similar information from the terminal as below but you can’t see LED toggled on the board because there is no led connected on the MCIMX93AUTO-EVK board .

Starting channel No.0 ...
 Channel No.0 interrupt is occurred !
 Channel No.0 interrupt is occurred !
 Channel No.0 interrupt is occurred !
 Channel No.0 interrupt is occurred !
 Channel No.0 interrupt is occurred !
 ........................