Hardware requirements
USB Type-C cable
MCIMX93-EVK board
Personal Computer
Board settings
To make the example work, connections needed to be as follows:
MASTER connect to SLAVE
Pin Name Board Location Pin Name Board Location
SCL J1005 pin 3 SCL J1005 pin 3
SDA J1005 pin 5 SDA J1005 pin 5
GND J1005 pin 7 GND J1005 pin 7
Note
Please run the application in Low Power boot mode (without Linux BSP). The IP module resource of the application is also used by Linux BSP. Or, run with Single Boot mode by changing Linux BSP to avoid resource conflict.
Prepare the Demo
Connect 12V~20V power supply and JLink Plus to the board, switch SW301 to power on the board
Connect a USB Type-C cable between the host PC and the J1401 USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either re-power up your board or launch the debugger in your IDE to begin running the demo.
Tips: The I3C use the same PHY pin as LPI2C, Acore already use the i2c resource. Please test the function in “LOW POWER MODE” only.
Running the demo
The following message shows in the terminal if the example runs successfully.
I3C board2board polling example -- Slave transfer.
Check I3C master I2C transfer.
Slave received data :
0x 1 0x20 0x 0 0x 1 0x 2 0x 3 0x 4 0x 5
0x 6 0x 7 0x 8 0x 9 0x a 0x b 0x c 0x d
0x e 0x f 0x10 0x11 0x12 0x13 0x14 0x15
0x16 0x17 0x18 0x19 0x1a 0x1b 0x1c 0x1d
0x1e 0x1f
I3C master I2C transfer finished .
Check I3C master I3C SDR transfer.
Slave received data :
0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7
0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f
0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17
0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f
I3C master I3C SDR transfer finished .