Hardware requirements
USB Type-C cable
MCIMX93-EVK board
J-Link Debug Probe
12V~20V power supply
Personal Computer
Board settings
Connect ADC channel0 (ADC_CH_00) to voltage supply which is 1.8v.
Connect ADC channel1 (ADC_CH_01) to voltage supply which is 1.65v.
Connect ADC channel2 (ADC_CH_02) to voltage supply which is 0.9v.
Please note this application can’t support running with Linux BSP!
Prepare the Demo
Connect 12V~20V power supply and J-Link Debug Probe to the board, switch SW301 to power on the board.
Connect a USB Type-C cable between the host PC and the J1401 USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either re-power up your board or launch the debugger in your IDE to begin running the example.
Running the demo
When the example runs successfully, you will see similar information from the terminal shown below.
ADC polling example.
Please press any key to get the conversion result.
The channel 0 ADC conversion data is 4084.
The channel 1 ADC conversion data is 3740.
The channel 2 ADC conversion data is 2049.
Please press any key to get the conversion result.
The channel 0 ADC conversion data is 4085.
The channel 1 ADC conversion data is 3741.
The channel 2 ADC conversion data is 2049.
Please press any key to get the conversion result.
The channel 0 ADC conversion data is 4084.
The channel 1 ADC conversion data is 3739.
The channel 2 ADC conversion data is 2049.