Hardware requirements

  • Mini/micro USB cable

  • MCX-N5XX-EVK Board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo

  1. Connect the micro and mini USB cable between the PC host and the USB ports on the board.

  2. Open a serial terminal on PC for the serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the example runs successfully, following information can be seen on the terminal:


==FlexCAN loopback example -- Start.==

Send message from MB0 to MB1
tx word0 = 0x11223344
tx word1 = 0x55667788

Received message from MB1
rx word0 = 0x11223344
rx word1 = 0x55667788

==FlexCAN loopback example -- Finish.==