Hardware requirements
Mini/micro USB cable
MCX-N5XX-EVK board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a USB cable between the host PC and the MCU-Link USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the demo runs successfully, the terminal will display similar information like the following:
Location is c00401
VOLATILE KEYS
ECC keys 224 bit ECC_KEY_PAIR(SECP_R1) with sign/verify algo ECDSA(SHA224): NOT SUPPORTED 521 bit ECC_KEY_PAIR(SECP_R1) with sign/verify algo ECDSA(SHA512): NOT SUPPORTED 256 bit ECC_KEY_PAIR(SECP_R1) with sign/verify algo ECDSA(SHA256): PASSED 256 ECC_KEY_PAIR(BRAINPOOL_R1) with sign/verify algo ECDSA(SHA256): NOT SUPPORTED 384 bit ECC_KEY_PAIR(BRAINPOOL_R1) with sign/verify algo ECDSA(SHA384): NOT SUPPORTED
AES keys 128 bit AES key with encrypt/decrypt algo ECB_NO_PADDING: PASSED 192 bit AES key with encrypt/decrypt algo CBC_NO_PADDING: NOT SUPPORTED 256 bit AES key with encrypt/decrypt algo CTR: PASSED 128 bit AES key with encrypt/decrypt algo CCM: NOT SUPPORTED 256 bit AES key with encrypt/decrypt algo GCM: PASSED 192 bit AES key with sign/verify algo CMAC : NOT SUPPORTED
MAC keys 256 bit PERSISTENT HMAC key with sign/verify algo HMAC(SHA-256): PASSED
RSA keys 2048 bit RSA key with sign/verify algo RSA_PKCS1V15(SHA256) : NOT SUPPORTED 2048 bit RSA key with sign/verify algo RSA_PSS(SHA512) : NOT SUPPORTED