Hardware requirements
Type-C USB cable
MCX-W72-EVK Board
Personal Computer
Board settings
No special is needed.
Prepare the Demo
Connect a mini USB cable between the PC host and the OpenSDA USB port on the board.
Open a serial terminal on PC for OpenSDA serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Please note, this example could only run on the EVK board.
Running the demo
When the example runs successfully, you can see the similar information from the terminal as below.
LPI2C example – Read Accelerometer Value Found an FXLS8964 on board , the device address is 0x19 . The accel values: x = 122 , y = 761 , z = 376 x = 122 , y = 761 , z = 376 x = 122 , y = 761 , z = 376 x = 125 , y = 680 , z = 470 x = 125 , y = 680 , z = 470 x = 163 , y = 664 , z = 708 x = 163 , y = 664 , z = 708 x = 102 , y = 657 , z = 931 x = 102 , y = 657 , z = 931 x = 102 , y = 657 , z = 931
End of LPI2C example.