Hardware requirements

  • Micro USB cable

  • MIMXRT685-AUD-EVK board

  • Personal Computer

Board settings

Prepare the Demo

  1. Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J5) on the board

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Launch the debugger in your IDE to begin running the demo.

Running the demo

When the example runs successfully, the following message is displayed in the terminal:

DMA channel chain example begin.
Destination Buffer:
0	0	0	0	0	0	0	0	0	0	0	0	0	0	0	0
DMA channel chain example finish.
Destination Buffer:
1	2	3	4	11	22	33	44 111 222 333 444	1111 2222 3333 4444