Hardware requirements
Type-C USB cable
MIMXRT700-EVK board
Personal Computer
Board settings
No special is needed.
Prepare the Demo
Connect a mini USB cable between the PC host and the MCU-Link USB port on the board.
Open a serial terminal on PC for MCU-Link serial device with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Reset the SoC and run the project.
Running the demo
When the demo runs successfully, the log would be seen on the MCU-Link terminal like:
USART CMSIS interrupt example
Board receives 8 characters then sends them out
Now please input:
When you input 8 characters, system will echo it by LPUART and them would be seen on the MCU-Link terminal.