Hardware requirements
Mini/micro USB cable
MIMXRT700-EVK board
Personal Computer
Board settings
The Multicore eRPC Two Way RPC RTOS project does not call for any special hardware configurations. Although not required, the recommendation is to leave the development board jumper settings and configurations in default state when running this demo.
Prepare the Demo
Connect the PC host and the board
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows the output of the eRPC Two Way RPC RTOS demo in the terminal window:
Primary core started
Get number from core1:
Got number: 1
Start normal rpc call example.
RPC call example finished.
Get number from core1:
Got number: 2
Start normal rpc call example.
RPC call example finished.
Get number from core1:
Got number: 3
Start normal rpc call example.
RPC call example finished.
.
.
.