Hardware requirements
Micro USB cable
RD-RW612-BGA board
Personal Computer
headphones with 3.5 mm stereo jack
Board settings
Connect JP50, JP51; Disconnect JP9, JP11
Prepare the Demo
Connect headphones to Audio HP connector (J4).
Connect a micro USB cable between the PC host and the MCU-Link USB port (J7) on the board
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Launch the debugger in your IDE to begin running the demo.
Running the demo
Headphones will play a sine wave sound. The log below shows example output of the I2S driver demo in the terminal window:
Configure codec
Configure I2S
Setup looping playback of sine wave