Overview

The ROM API project is a simple demonstration program of the SDK ROM API driver.

  • The ROM API supports native support for callable crypto functions in the user application.

Hardware requirements

  • Micro USB cable

  • RD-RW612-BGA board

  • Personal Computer

Board settings

No special settings are required.

Prepare the Demo

  1. Connect a micro USB cable between the PC host and the MCU-Link USB port (J7) on the board

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Launch the debugger in your IDE to begin running the demo.

Running the demo

This example will run NBOOT apis. When the example runs successfully, the following message is displayed in the terminal.

ROM API NBOOT Driver
INFO: Starting Example test_nboot_context_init
INFO: Finished Example test_nboot_context_init
INFO: Starting Example test_romapi_rng_generate_random
 data_buf[0] random num
 data_buf[1] random num
 data_buf[2] random num
 data_buf[3] random num
INFO: Finished Example test_romapi_rng_generate_random
INFO: Starting Example test_nboot_context_deinit
INFO: Finished Example test_nboot_context_deinit
ALL nboot examples completed successfully!