Hardware requirements
Micro USB cable
RD-RW612-BGA board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a micro USB cable between the PC host and the MCU-Link USB port (J7) on the board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Launch the debugger in your IDE to begin running the example.
Running the demo
When the demo runs successfully, the terminal will display similar information like the following:
ELS PKC asymmetric cipher example
============================ PKC ECC keygen sign verify:pass PKC RSA no-verify:pass PKC RSA sign no-encode:pass PKC RSA-PSS sign SHA256:pass PKC RSA-PSS verify SHA256:pass PKC ECC Curve25519:pass TLS Master session keys:pass
============================ RESULT: All 7 test PASS!! ELS example END