Hardware requirements

  • Micro USB cable

  • TWR-KM35Z75M board

  • Personal Computer

Board settings

I2C one board:

  • Transfer data from MASTER_BOARD to SLAVE_BOARD of I2C interface, I2C0 pins of MASTER_BOARD are connected with I2C0 pins of SLAVE_BOARD

MASTER_BOARD        CONNECTS TO          SLAVE_BOARD
Pin Name   Board Location     Pin Name   Board Location
I2C0_SCL       J25-12         I2C0_SCL      J25-12
I2C0_SDA       J25-11         I2C0_SDA      J25-11
GND            J25-10         GND           J25-10

Prepare the Demo

  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

When the demo runs successfully, the following message is displayed in the terminal:

I2C board2board interrupt example – Master transfer. Master will send data : 0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7 0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f 0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17 0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f

Receive sent data from slave : 0x 0 0x 1 0x 2 0x 3 0x 4 0x 5 0x 6 0x 7 0x 8 0x 9 0x a 0x b 0x c 0x d 0x e 0x f 0x10 0x11 0x12 0x13 0x14 0x15 0x16 0x17 0x18 0x19 0x1a 0x1b 0x1c 0x1d 0x1e 0x1f

End of I2C example .