Hardware requirements

  • Mini USB cable

  • TWR-MC56F8200 board

  • Personal Computer

Board hardware common setting

  1. HW reworkd(workaround):

    Connect J18(the mini USB port) pin4 and pin5. Note: This is due to HW design error, correct setting should be: J18 pin4 left empty and pin5 connected GND.

  2. Power setting:

    Connect J11 pin1 and pin2 Connect J6 pin1 and J7 pin2

  3. UART setting:

    Connect J8 pin3 and pin4 Connect J9 pin3 and pin4

  4. Onboard OSJTAG debugger setting:

    Connect J20 pin1 and pin2. Leave J17 open. Note: J17 is only used(connected) when firmware update for onboard debugger OSJTAG. Connect J21 pin 1-2, 3-4, 5-6, 7-8, to setup onboard debugger OSJTAG. Note: when use external debugger(connected to J14), leave all J21 pins open

Board settings

  • Pull-up SCL/SDA each to 3.3V with resistor(2.2K~5.1K ohm)

    MASTER_BOARD connects to SLAVE_BOARD as below:

    MASTER_BOARD        CONNECTS TO         SLAVE_BOARD
    Pin Name   Board Location     Pin Name   Board Location
    I2C0_SCL   J501-21            I2C0_SCL   J501-21
    I2C0_SDA   J501-23            I2C0_SDA   J501-23
    GND        J501-8             GND        J501-8
    

Prepare the Demo

  1. Connect USB cable between the host PC and the JM60 USB(J18) port on the target board. It setups OSJTAG and COM port in PC device manager.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board with OSJTAG debug configuration.

  4. Launch the debugger in your IDE to begin running the demo.

Running the demo

When the example runs successfully, you can see the similar information from the terminal as below.

I2C board2board interrupt example -- Master transfer.
Master will send data :
0x 0  0x 1  0x 2  0x 3  0x 4  0x 5  0x 6  0x 7  
0x 8  0x 9  0x a  0x b  0x c  0x d  0x e  0x f  
0x10  0x11  0x12  0x13  0x14  0x15  0x16  0x17  
0x18  0x19  0x1a  0x1b  0x1c  0x1d  0x1e  0x1f  

Receive sent data from slave :
0x 0  0x 1  0x 2  0x 3  0x 4  0x 5  0x 6  0x 7  
0x 8  0x 9  0x a  0x b  0x c  0x d  0x e  0x f  
0x10  0x11  0x12  0x13  0x14  0x15  0x16  0x17  
0x18  0x19  0x1a  0x1b  0x1c  0x1d  0x1e  0x1f  


End of I2C example .
~~~~~~~~~~~~~~~~~~~~~~~~~~~~