Plugin boot application
The plugin boot application is usually used to enable boot features that are not natively supported by Boot ROM, for example,
Boot from USB disk
Boot from Ethernet,
DDR/SDRAM configuration
Redundant boot/reliable boot
The prototype of plugin boot application is:
bool (*plugin_download)(void **start, size_t *bytes, uint32_t *ivt_offset);
Principles for Plugin boot application design
The Boot ROM needs to jump between Plugin boot image and the normal boot image that is loaded by the plugin boot application. To avoid any impact on the ROM boot flow, here are some recommended principles for plugin boot application design.
The plugin boot application must not use the memory that is currently reserved for ROM use
The plugin boot application should use minimum stack spaces to avoid the possibility of stack overflow caused by plugin boot application
The plugin boot application must consider Watchdog service, if the WDOG enable bit is enabled in the Fuse block
Parent topic:Plugin boot application
Boot Flow of Plugin boot application
The boot flow for Plugin boot application is as follows
Boot ROM loads the XIP plugin boot image, does authentication and execution and then jump to plugin boot application
The plugin boot application loads the signed Non-XIP image from address 0x60008000 and jumps back to Boot ROM
Boot ROM does authentication/decryption based on the parameters output by plugin boot application and jumps to the non-XIP boot image after authenticating successfully
Parent topic:Plugin boot application
Example Plugin boot application to enable non-XIP boot on FlexSPI NOR
The Non-XIP boot case is not natively supported by some i.MX RT Boot ROM devices. In this case, a simple plugin boot image can be created to enable non-XIP boot case for these boot devices.
The basic flow of how Plugin boot works is as follows:
Here are the example codes for plugin boot application for RT10xx FlexSPI NOR boot.
#define BOOT_IMAGE_LOAD_BASE 0x60008000
enum
{
kTag_HAB_IVT = 0xd1,
};
typedef struct _hab_hdr
{
uint8_t tag;
uint8_t len[2];
uint8_t version;
} hab_hdr_t;
typedef struct _hab_ivt
{
hab_hdr_t hdr;
uint32_t entry;
uint32_t reserved1;
uint32_t dcd;
uint32_t boot_data;
uint32_t self;
uint32_t csf;
uint32_t reserved2;
} hab_ivt_t;
//!@brief Boot data structure
typedef struct _boot_data
{
uint32_t start;
uint32_t length;
uint32_t plugin;
uint32_t reserved;
} boot_data_t;
//!@brief Boot Image header, including both IVT and BOOT_DATA
typedef struct _boot_image_hdr
{
hab_ivt_t ivt;
boot_data_t boot_data;
} boot_image_hdr_t;
/*!@brief Plugin Download function
*
* This function is used to copy non-xip boot image from Flash to RAM
*
*/
bool plugin_download(void **start, size_t *bytes, uint32_t *ivt_offset)
{
bool result = false;
const boot_image_hdr_t *boot_hdr;
//Search IVT
uint32_t ivt_offset_list[3] = {0, 0x400, 0x1000};
uint32_t search_index = 0;
while (search_index < sizeof(ivt_offset_list) / sizeof(ivt_offset_list[0]))
{
boot_hdr = (const boot_image_hdr_t *)(ivt_offset_list[search_index] +
BOOT_IMAGE_LOAD_BASE);
if (boot_hdr->ivt.hdr.tag != kTag_HAB_IVT)
{
search_index++;
continue;
}
*start = (void *)boot_hdr->boot_data.start;
*bytes = boot_hdr->boot_data.length;
*ivt_offset = boot_hdr->ivt.self - boot_hdr->boot_data.start;
uint32_t *dst = (uint32_t *)boot_hdr->boot_data.start;
uint32_t *src = (uint32_t *)((uint32_t)boot_hdr - *ivt_offset);
size_t remaining_length = ((*byte + 3) & ~0x03) / 4;
while (remaining_length--)
{
*dst++ = *src++;
}
result = true;
break;
}
return result;
}
Parent topic:Plugin boot application
Images loaded by plugin boot application
The image loaded by Plugin boot application can be either XIP image or the non-XIP image. Refer to Chapter 4, Generate i.MX RT bootable image for more details.
Parent topic:Plugin boot application
Parent topic:Appendix