Beacon filtering guidelines

A filter can be introduced for filtering beacons in network searches (on a Router or End Device). Beacons can be filtered on the basis of Extended PAN ID (EPID), LQI value and device joining status/capacity (see below). The filter can be applied using the function ZPS_bAppAddBeaconFilter().

If required, the above function must be called immediately before ZPS_eAplZdoDiscoverNetworks(), ZPS_eAplZdoRejoinNetwork() or ZPS_eAplZdoStartStack().

A tsBeaconFilterTypestructure is supplied to the ZPS_bAppAddBeaconFilter()

function in order to specify the details of the filter to be implemented, including:

  • A blacklist or whitelist of networks in terms of a list of EPIDs.

  • The PAN ID of the network from which acceptable beacons should come.

  • The minimum LQI value of an acceptable beacon.

  • Flags indicating the properties on which beacons will be filtered, which include:

    • LQI value of beacon.

    • Permit Join enabled on sending device.

    • Capacity of sending device to accept Router children.

    • Capacity of sending device to accept End Device children.

After each discovery or rejoin, the flags are cleared while all other fields of the structure remain intact. The structure is detailed in Section 8.2.3.5.

The following general guidelines should be followed in using beacon filters:

  • Do not implement a filter unless attempting a join, as this would prevent some stack operations from working correctly.

  • Do not enable a blacklist and whitelist at the same time.

  • Do not declare your filter structure as a local variable in a function, as it needs to exist for the duration of the discovery.

The following guidelines are relevant to network rejoins and associations.

Network rejoin

  • Do set up a whitelist containing a single EPID corresponding to the network that the node is to rejoin (if only one network is of interest) and/or the PAN ID of this network.

  • Do set up an LQI filter to reject distant beacons, if required.

  • Do not enable filtering on Permit Join or Router/End Device Capacity.

Parent topic:Beacon filtering guidelines

Association

  • Do set up an LQI filter to reject distant beacons, if required.

  • Do filter on the Permit Join status to only find potential parents and networks that are accepting association requests.

  • Do filter on Router/End Device Capacity, if required, depending on device type.

Note: A blacklist can be built up over several attempts to discover and associate, by keeping on adding to the array of EPIDs, as each network is rejected.

Parent topic:Beacon filtering guidelines

Parent topic:Appendix B: Application design notes