Build an example application

To build an example application, follow these steps.

  1. Drag and drop the SDK zip file into the Installed SDKs view to install an SDK. In the window that appears, click OK and wait until the import has finished.

  2. On the Quickstart Panel, click Import SDK example(s)….

  3. In the window that appears, select frdmimxrt1186 and click Next.

  4. Expand the demo_apps folder and select hello_world_demo_cm33. Then, click Next.

  5. Click Finish.

Parent topic:Run a demo using MCUXpresso IDE