MCUXpresso SDK Integration

McuxSDK CMake Package

MCUXpresso SDK can be used as a standard McuxSDK CMake package . It ensures that CMake can automatically find the MCUXpresso SDK and use it to build the example.

There are 2 ways to use the McuxSDK CMake package:

  1. Export the MCUXpresso SDK to system standard CMake user package registry and directly use find_package(McuxSDK).

    Here is the table about the standard CMake user package registry in different OSes.

    OS

    CMake user package registry

    Windows

    HKEY_CURRENT_USER\Software\Kitware\CMake\Packages\McuxSDK

    Linux

    ~/.cmake/packages/McuxSDK

    MacOS

    ~/.cmake/packages/McuxSDK

    There are 2 ways to export MCUXpresso SDK repo.

    1. You can use west cmd west mcuxsdk-export to export.

    2. You can directly use cmake cmd cmake -P <sdk repo root>/share/mcuxsdk-package/cmake/mcuxsdk_export.cmake to export.

  2. Directly add the MCUXpresso SDK root as HINT for find_package(McuxSDK HINT <repo root>)

Create Example With find_package(McuxSDK)

When using McuxSDK CMake package, you just simply needs to write find_package(McuxSDK) at the beginning of the application CMakeLists.txt file, then build system will get all needed drivers, components and middlewares for designated devices and boards and build them into a static library called McuxSDK. This McuxSDK has been linked to target app in advance, you only need to add the example specific sources/include/configuration.

Here is an example:

cmake_minimum_required(VERSION 3.30.0)
find_package(Mcuxsdk REQUIRED)
project(hello_world LANGUAGES C CXX ASM)
mcux_add_source(
  SOURCES   
    hello_world.c
    hardware_init.c
    app.h
)
mcux_add_include(
  INCLUDES 
    .
)

If you use native cmake target_ function with target app, then the sources/includes/configurations are added for target app. If you use NXP cmake extension to add sources/includes/configurations, then the data and files are added into target McuxSDK, a static library, which will be linked to app finally.

If there is no special instruction, the app target will use default provided linker script by MCUXpresso SDK if it is an executable. If it doesn’t satisfy your needs, then please add CUSTOM_LINKER TRUE in the project like the following and then add your own linker script.

project(hello_world LANGUAGES C CXX ASM CUSTOM_LINKER TRUE)

There is no PROJECT_BOARD_PORT_PATH support in this find_package(McuxSDK)way which means you need to provide your own board port files, typically hardware_init.c and app.h, and disable the original ones in prj.conf. So the example dedicated prj.conf will have following lines:

CONFIG_MCUX_HAS_PRJSEG_project.use_hw_app=n
CONFIG_MCUX_PRJSEG_project.hw_app_project_folder=n
CONFIG_MCUX_PRJSEG_module.board.pinmux_board_folder=y

The CONFIG_MCUX_PRJSEG_module.board.pinmux_board_folder=y guarantee that the example is using board level pin_mux because default enabled is pin_mux located in project root.

We provide a frdmmcxa346 hello_world find_package(McuxSDK) example for reference.

for reference.

McuxSDK CMake Package Version

find_package(McuxSDK) supports to specify MCUXpresso SDK version number in x.y.z format which is very useful as it ensures the example is built with a minimal MCUXpresso SDK version. An explicit version also helps CMake to select the correct MCUXpresso SDK to use for building when there are multiple MCUXpresso SDK repositories in the system.

Here is an example with version:

find_package(McuxSDK 3.0.0)
project(hello_world)

This requires hello_world project to be built with MCUXpresso SDK version 3.0.0 as minimum.

find_package supports the keyword EXACT to ensure an exact version is used.

find_package(McuxSDK 3.0.0 EXACT)
project(hello_world)

Integrated Into Other Build System

Import as CMake package

If you want to integrate the MCUXpresso SDK to your project by CMake find_package feature, please refer the above McuxSDK CMake Package.

Import manually

The MCUXpresso SDK can also be integrated by adding cmake file manually. You need to load ${SdkRootDirPath}/cmake/extension/mcux.cmake before project declaration, and load ${SdkRootDirPath}/CMakeLists.txt after project declaration. For example:

cmake_minimum_required(VERSION 3.30.0)

include(${SdkRootDirPath}/cmake/extension/mcux.cmake)

project(hello_world LANGUAGES C CXX ASM)

include(${SdkRootDirPath}/CMakeLists.txt)

mcux_add_source(
  SOURCES   
    hello_world.c
    pin_mux.c
    pin_mux.h
    hardware_init.c
    app.h
)

mcux_add_include(
  INCLUDES .
)

Build the project

There are 2 ways to build the project:

  1. With cmake command

  cmake -B ./build -G Ninja -Dboard=<board> -DCONF_FILE=<Absolute path to project folder>/prj.conf -DCMAKE_BUILD_TYPE=debug -DCONFIG_TOOLCHAIN=armgcc

  ninja -C build
  1. With west command

  west build -b <board> <Absolute/relative path to project folder> -DCONF_FILE=<Absolute path to project folder>/prj.conf --config=debug --toolchain=armgcc

Furthermore, if you encounter an error like below with west build command, one possible reason is the project is added to other project by add_subdirectory, that’s the limitation from west, please skip the sanity check by adding west parameter -nsc or --no_sanity_check

Build directory <A> is for application <B>, but source directory <C> was specified; please clean it, use --pristine, or use --build-dir to set another build directory

Currently GUI project and standalone project generation are not supported for other build system which uses McuxSDK CMake Package.

Integrate Other CMake Build System

The MCUXpresso SDK build system is based on CMake, so theoretically, it supports the integration of other third-party software based on the CMake compilation system.

There are two ways for this requirement:

  1. If the third-party software needs to be built as a library and linked to the project from MCUXpresso SDK build system, you can add the software path to cmake variable EXTRA_MCUX_MODULES. The directory of the path will be treated as the module’s name. You need to create a folder named mcux in this path, and prepare files below:

    • module.yml

      module.yml must be put into mcux folder. It records the relative path of CMakeLists.txt and Kconfig file. Note that the base path is the path form EXTRA_MCUX_MODULES. For example:

      name: zcbor #optional, must be set only if module folder name is different with module name
      build:
        # if the base path is ~/zcbor
        cmake: mcux/.             #full path ~/zcobr/mcux/CMakeLists.txt
        kconfig: mcux/Kconfig     #full path ~/zcobr/mcux/Kconfig
        depends:                 # optional, dependent module will be included into the build system and be processed before current module.
          - <module>
      
    • Kconfig

      At least one Kconfig item MCUX_COMPONENT_${module_name} should be recorded to help enable/disable the third-party software from building. For example:

      config MCUX_COMPONENT_ZCBOR
          bool "zcbor CBOR library"
          help
            zcbor CBOR encoder/decoder library
      
      if MCUX_COMPONENT_ZCBOR
      
      config ZCBOR_CANONICAL
          bool "Produce canonical CBOR"
          help
            Enabling this will prevent zcbor from creating lists and maps with
            indefinite-length arrays (it will still decode them properly).
      endif # MCUX_COMPONENT_ZCBOR  
      
    • CMakeLists.txt

      All content should be wrapped by if(CONFIG_MCUX_COMPONENT_${module_name}) ... endif(). Then we can enable/disable the third-party software according to kconfig setting. There is no strict format for CMakeLists.txt. The module project will be linked to application code automatically by build system if it is a static library.

      For example:

      cmake_minimum_required(VERSION 3.20.0)
      
      if(CONFIG_MCUX_COMPONENT_ZCBOR)
          add_library(zcbor) # declare a zcbor library 
      
          target_sources(zcbor PRIVATE # add files to zcbor library
                  ${MCUX_ZCBOR_MODULE_DIR}/src/zcbor_common.c
                  ${MCUX_ZCBOR_MODULE_DIR}/src/zcbor_decode.c
                  ${MCUX_ZCBOR_MODULE_DIR}/src/zcbor_encode.c
          )
      
          target_include_directories(zcbor PUBLIC # add include path to zcbor library
                  ${MCUX_ZCBOR_MODULE_DIR}/include
          )
      
          target_compile_definitions(zcbor PUBLIC _POSIX_C_SOURCE=200809L) # add macro to zcbor library and the targets which links this library
      
          if(CONFIG_ZCBOR_CANONICAL)
              target_compile_definitions(zcbor PRIVATE ZCBOR_CANONICAL) # # add macro only for zcbor library 
          endif ()
      
      endif()
      

The software will use assembler/compiler/linker flags provided by MCUXpresso SDK build system, you can also set specific options for the third-party software in PRIVATE scope. If the module is a library project, MCUXpresso SDK build system can link the library automatically.

Due to the loading sequence of cmake files, the compilation settings in reconfig.cmake are not available, so if necessary, you need to set them yourself in CMakeLists.txt of the module.

  1. If the other software is a standalone project which has separated configuration, it can be imported by sysbuild.

    For example, you can provide a sysbuild.cmake:

    ExternalMCUXProject_Add(
            APPLICATION my_library
            SOURCE_DIR  path/to/my_library
            CMAKE_ARGS -DCMAKE_BUILD_TYPE=debug -DCMAKE_TOOLCHAIN_FILE=path/to/toolchain.cmake
    )
    
    # Let's build the secondary application first
    add_dependencies(${DEFAULT_IMAGE} my_library)