Hardware requirements
Micro USB cable
MIMXRT1060-EVKC board
Personal Computer
Headphone or speaker
CS42448 audio board
Line in line
Board settings
Insert AUDIO board into J23
If use MIC as input, please remove J99
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Insert the CS42448 audio board into J23.
Insert the headphones into the headphone jack of CS42448 audio board line output.
Connect the audio input source to the CS42448 audio board by line in line.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
Note: The Stereo input 1 will playback through Line 1&2 output. The Stereo input 2 will playback through Line 3&4 output. The MIC input 1&2 will playback through Line 5&6 output.
SAI TDM record playback example started!
Codec Init Done.