Overview
The fsl_romapi example shows how to use ROM API:
In this example, fsl_romapi driver will call the API and operate the external Nor flash connected to the FLEXSPI controller. Some simple flash command will be executed, such as FLEXSPI NOR get config, FLEXSPI NOR Flash init, Erase sector, Program page. Example will first erase the sector and program a page into the flash, at last check if the data in flash is correct.
Hardware requirements
Mini/micro USB cable
FRDM-IMXRT1186 board
Personal Computer
Board settings
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the example runs successfully, you can see the similar information from the terminal as below.
For FLEXSPI NOR targets, the result is:
FLEXSPI NOR example started!
Successfully get FLEXSPI NOR configuration block
Successfully init FLEXSPI serial NOR flash
Serial NOR flash has been found successfully
Vendor ID: xx
Serial NOR flash Information:
Total program flash size: xx KB, Hex: (xx)
Program flash sector size: xx KB, Hex: (xx)
Program flash page size: xx B, Hex: (xx)
Erasing serial NOR flash over FLEXSPI
Successfully erased one sector of NOR flash device xx -> xx
Program a buffer to a page of NOR flash
Successfully programmed and verified location FLEXSPI memory xx -> xx
End of FLEXSPI NOR Example!