Hardware requirements
Mini/micro USB cable
FRDM-IMXRT1186 board
Personal Computer
Board settings
J18(1-2)/J17(2-3): ETH2 Function Via J56B. J12(1-2)/J13(2-3): ETH0 Function Via J56A.
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the demo runs successfully, the log would be seen on the OpenSDA terminal like:
NETC Switch example start.
Wait for PHY link up...
MAC learning.
The frame received from port 0. Dest Address 54:27:8d:00:00:f0 Src Address 54:27:8d:00:00:00. Port 0 bounds to MAC 54:27:8d:00:00:00.
The frame received from port 2. Dest Address 54:27:8d:00:00:f0 Src Address 54:27:8d:00:00:02. Port 2 bounds to MAC 54:27:8d:00:00:02.
Frame forwarding.
The frame received from pseudo port. Dest Address 54:27:8d:00:00:00 Src Address 54:27:8d:00:00:f0. Frame forwarding to port 0.
The frame received from pseudo port. Dest Address 54:27:8d:00:00:02 Src Address 54:27:8d:00:00:f0. Frame forwarding to port 2.