Hardware requirements
Mini/micro USB cable
FRDM-IMXRT1186 board
Personal Computer
Board settings
Prepare the Demo
Connect a USB cable between the PC host and the OpenSDA USB port on the board.
Open a serial terminal with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the example.
Running the demo
When the example runs successfully, the following message is displayed in the terminal:
TMPSNS driver example. 
The chip initial temperature is 23.4 ℃. 
The chip temperature has reached high temperature that is 30.9 ℃. 
~~~~~~~~~~~~~~~~~~~~~~~
Note 1:
To run this exmaple successfully, you should heating the chip outside, such as blowing heating.