Hardware setup
Hardware requirements
FRDM-IMXRT1186 RevC
RJ45 Network cable
Mini/micro USB cable
Personal computer with TwinCat3.(Windows 10 is recommended)
Board settings
The board does not require any special settings.
Connection
Connect the EtherCAT Port 0 (J28 RJ45 interface) on the FRDM-IMXRT1186 board with TwinCAT3 via the Ethernet cable.
Connect a USB cable between the host PC and the OpenSDA USB port on the FRDM-IMXRT1186 board.
Open a serial terminal with the following settings.
115,200 baud rate
8 data bits
No parity
One stop bit
No flow control