Hardware requirements
Micro USB cable
FRDM-KE16Z board
Personal Computer
Board settings
This example project uses ADC12 instance 0 to sample and convert the voltage signal input from channel 0(PTA0). So the voltage signal input from PTA0(J4-12) should be changed to observe the dynamical conversion result.
Prepare the Demo
Connect a USB cable between the PC host and the OpenSDA USB port on the board.
Open a serial terminal with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the example.