Hardware requirements
Micro USB cable
FRDM-KE17Z board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the example.
Running the demo
When the example runs successfully, the following message is displayed in the terminal
 PFlash Example Start 
 PFlash Information: 
 Total Program Flash Size:	256 KB, Hex: (0x40000)
 Program Flash Sector Size:	2 KB, Hex: (0x800) 
 Flash is UNSECURE!
 Erase a sector of flash
 Successfully Erased Sector 0x3f800 -> 0x40000
 Program a buffer to a sector of flash 
 Successfully Programmed and Verified Location 0x3f800 -> 0x3f810 
 End of PFlash Example