Hardware requirements
Type-C USB cable
FRDM-MCXA344 board
Personal Computer
Board settings
No special settings are required.
Prepare the Demo
Connect a USB Type-C cable between the host PC and the LPC-Link USB port (P6) on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
When the example runs successfully, the following message is displayed in the terminal:
Calling the runBootloader API to force into the ISP mode: x...
The runBootloader ISP interface is choosen from the following one:
kIspPeripheral_Auto : 0
kIspPeripheral_UsbHid : 1
kIspPeripheral_Uart : 2
kIspPeripheral_SpiSlave : 3
kIspPeripheral_I2cSlave : 4
kIspPeripheral_Can : 5
Call the runBootloader API based on the arg : xxxxxxxx...