Hardware requirements

  • Mini/micro USB cable

  • FRDM-MCXE31B board

  • Personal Computer

Board settings

Prepare the Demo

  1. Connect a USB-C cable between the PC host and the MCU-Link USB port on the board

  2. Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.