Hardware requirements
Type-C USB cable
FRDM-MCXN947 board
Personal Computer
Board settings
Attach OV7670 to J9 camera interface(pin5 to pin22). Rework the camera pins by changing the SJ16, SJ26 and SJ27 from right side to left side. Attach LCD-PAR-S035 low cost panel to J8.
Prepare the Demo
Connect a type-c USB cable between the PC host and the MCU-Link USB port (J17) on the board
Open a serial terminal with the following settings (See Appendix A in Getting started guide for description how to determine serial port number):
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.