Hardware requirements
Type-C USB cable
KW47-LOC Board
Personal Computer
Board settings
Prepare the Demo
Connect a USB cable between the host PC and UART1 on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
Copyright 2024 NXP
LOG SHELL>>