Hardware requirements
Type-C USB cable
KW47-LOC Board
Personal Computer
Board settings
No special is needed.
Prepare the Demo
Connect a USB cable between the host PC and the LOC board J3.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.
Running the demo
The log below shows the output of the demo in the terminal window:
............................. LTC (AES) DRIVER EXAMPLE .............................
Testing input string:
Once upon a midnight dreary, while I pondered weak and weary,
Over many a quaint and curious volume of forgotten lore,
While I nodded, nearly napping, suddenly there came a tapping,
As of some one gently rapping, rapping at my chamber door
Its some visitor, I muttered, tapping at my chamber door
Only this, and nothing more.
----------------------------------- AES-CBC method --------------------------------------
AES CBC Encryption of 320 bytes.
AES CBC encryption finished.
AES CBC Decryption of 320 bytes.
AES CBC decryption finished.
Decrypted string :
Once upon a midnight dreary, while I pondered weak and weary,
Over many a quaint and curious volume of forgotten lore,
While I nodded, nearly napping, suddenly there came a tapping,
As of some one gently rapping, rapping at my chamber door
Its some visitor, I muttered, tapping at my chamber door
Only this, and nothing more.
----------------------------------- AES-CCM method --------------------------------------
AES CCM Encryption of 320 bytes.
using iv length : 12 bytes
using aad length : 20 bytes
using key length : 16 bytes
using tag length : 8 bytes
AES CCM encryption finished.
AES CCM decryption of 320 bytes.
AES CCM decryption finished.
Decrypted string:
Once upon a midnight dreary, while I pondered weak and weary,
Over many a quaint and curious volume of forgotten lore,
While I nodded, nearly napping, suddenly there came a tapping,
As of some one gently rapping, rapping at my chamber door
Its some visitor, I muttered, tapping at my chamber door
Only this, and nothing more.
----------------------------------- AES-CMAC ------------------------------------------
AES CMAC Computing hash of 320 bytes
Computed hash:
ba fd 2c 65 a 62 7c 18 a0 df b4 20 bb fb 68 27
.............. THE END OF THE LTC (AES) DRIVER EXAMPLE ................................