Hardware requirements
Micro USB cable
LPCXpresso860max board
Personal Computer
Board settings
ADC CH0 input signal J6-12(PIO0-7).
Prepare the Demo
Connect a micro USB cable between the PC host and the CMSIS DAP USB port (J4) on the board
Open a serial terminal with the following settings:
9600 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Press reset button to begin running the demo.
Running the demo
Monitor the information on the debug console.
Expected Result
Press any key and print user channel’s result in serial terminal.