Hardware requirements

  • Type-C USB cable

  • Personal Computer

  • MCXW72-LOC board

Board settings

No special settings are required.

Prepare the Demo

  1. Connect a USB cable between the host PC and the LOC board J3.

  2. Open a serial terminal on PC for the serial device with these settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.

Running the demo

The following lines are printed to the serial terminal when the demo program is executed.

Producer_task created.
Consumer_task 0 created.
Consumer_task 1 created.
Consumer_task 2 created.
Consumer number: 0
Consumer 0 accepted item.
Consumer number: 1
Consumer number: 2
Producer released item.
Consumer 0 accepted item.
Producer released item.
Consumer 1 accepted item.
Producer released item.
Consumer 2 accepted item.