Hardware requirements

  • Mini USB cable

  • TWR-KM34Z50MV3 board

  • Personal Computer

Board settings

The connection should be set as following:

  • J33 no shunt on

Prepare the Demo

  1. Connect a USB cable between the host PC and the OpenSDA USB port on the target board.

  2. Open a serial terminal with the following settings:

    • 115200 baud rate

    • 8 data bits

    • No parity

    • One stop bit

    • No flow control

  3. Download the program to the target board.

  4. Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.