Hardware requirements
Mini USB cable
TWR-KM34Z75M board
Personal Computer
Board settings
The connection should be set as following:
J33 no shunt on
Prepare the Demo
Connect a USB cable between the host PC and the OpenSDA USB port on the target board.
Open a serial terminal with the following settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Download the program to the target board.
Either press the reset button on your board or launch the debugger in your IDE to begin running the demo.