cop
Overview
The COP Example project is to demonstrate usage of the KSDK cop driver. In this example, after 10 times of refreshing, a timeout reset is generated. Please notice that because COP control registers are write-once only, so the COP_Init function and the COP_Disable function can be called only once after reset. In SystemInit() function which is called in startup code, there is an operation to disable the watchdog if macro DISABLE_WDOG is defined as 0, and by default if the DISABLE_WDOG is not defined, the DISABLE_WDOG is defined as 1. So this example has a special project setting that defines the DISABLE_WDOG macro to 0 so the startup code will skip the disable COP WDOG operation.
Since IAR debug setting will by default disable the COP WDOG, so example provide a mac file to skip this disable operation for IAR.