modbus_rtu_client
Overview
This example demonstrates how to use Modbus RTU protocol to communication.
FreeModbus supports bellow feature:
Read coil(0x01)
Read discrete inputs(0x02)
Read holding registers(0x03)
Read input registers(0x04)
Write single coil(0x05)
Write single holding register(0x06)
Write board LED status(0x0d)
Read board LED status(0x0e)
Write multiple coils(0x0f)
Write multiple holding registers(0x10)
Running the demo
If the test passes, serial port output:
Modbus RTU Client Example Start!
Use the MIMXRT1180-EVK board as modbus Server simulator, write board LED status(0x0d) to control LED(D6, D7) light