host_cdc_ecm
Overview
The host CDC-ECM project is a simple demonstration program based on the MCUXpresso SDK . It demonstrates Ping and UDP echo server, it also join into a multicast group. The application periodically sends the ICMP echo request to a PC and processes the PC reply and always forwarding UDP message on echo port.
System Requirement
Hardware requirements
Mini/micro USB cable
USB A to micro AB cable
Hardware (Tower module/base board, and so on) for a specific device
Personal Computer (PC)
Software requirements
The project path is:
<MCUXpresso_SDK_Install>/boards//usb_examples/usb_host_cdc_ecm/ / . 
The
is Bare Metal or FreeRTOS OS. 
Getting Started
Hardware Settings
For detailed instructions, see the appropriate board User’s Guide.
Set the hardware jumpers (Tower system/base module) to default settings.
Prepare the example
Connect a USB cable between the PC host and the USB port on the target board with these settings:
115200 baud rate
8 data bits
No parity
One stop bit
No flow control
Make sure to use a USB HUB or an adapter with OTG functionality firstly. Connect the target board to the external power source (the example is self-powered).
Download the program to the target board.
Power off the target board, then power on again.
For detailed instructions, see the appropriate board User’s Guide.
Run the example
Connect serial port to board and run the example host_cdc_ecm , then plug in USB CDC-ECM device to the board. The log will printed like below:

If network link of CDC-ECM device is up, the example host_cdc_ecm will start DHCP service and join into a multicast group using IGMP. The example host_cdc_ecm will always listening on UDP port 7 and echo message to sender, then start Ping. The log will printed like below:

Supported Boards
MCX-N5XX-EVK
MCX-N9XX-EVK
FRDM-MCXN947
RD-RW612-BGA
FRDM-RW612