Logo
25.09.00-pvw2
MCUXpresso SDK Project v: latest
Document Release Versions
25.09.00-pvw2
25.09.00-pvw1
25.06.00
25.06.00-pvw2
25.06.00-pvw1
latest

Introduction

  • MCUXPresso SDK

Getting Started

  • Github Repository
  • Zip Package

User Guide

  • Drivers
  • Examples
  • Middleware
  • RTOS
  • Boards

Development

  • Build And Configuration System
  • Developing with MCUXpresso SDK

Releases

  • Release Notes
mcuxsdk
  • Docs »
  • Link cost
  • Open on Repo Report an issue

Link cost

For the purpose of packet filtering, LQI values are translated into ‘link cost’ values. Thus, a range of LQI values maps to a single link cost, which is an integer value. The default mappings implemented by the ZigBee PRO stack are shown in the table below.

‘LQI to Link Cost’ Mappings

LQI Range

Link Cost

≥ 51

1

46 - 50

2

41 - 45

3

39 - 40

4

36 - 38

5

25 - 35

6

≤ 24

7

The above mappings can be modified, as described in Section 6.10.3.3. A link cost of 5 is used as the packet filtering threshold by the NXP ZigBee PRO stack. Thus, packets with link costs greater than 5 may be discarded. For the device, this threshold is more suitable than the value of 3 proposed in the ZigBee specification. However, the threshold is configurable, as described in Section 6.10.3.3.

Parent topic:Filtering packets on LQI Value/Link cost


Copyright 2025, NXP. Last generated on Aug 12, 2025 21:36+0200; branch release/25.09.00-pvw2, revision a3dbcfa94de3d9565ba3c17feed5286d9564bdbe.