Light Level Sensor
The Light Level Sensor device measures the illumination level in an area. It can be used to switch on/off a lighting device, such as an On/Off Ballast.
The Device ID is 0x010E.
The header file for the device is light_level_sensor.h.
The clusters supported by the device are listed in Section 3.15.1.
The device structure,
tsZLO_LightLevelSensorDevice, is listed in Section 3.15.2.The endpoint registration function for the device, eZLO_RegisterLightLevelSensorEndPoint(), is detailed in Section 3.15.3.
Supported clusters
The clusters used by the Light Level Sensor device are listed in the table below.
Table 20. Clusters for Light Sensor |
|
|---|---|
Server (input) side |
Client (output) side |
Mandatory |
|
Basic |
Identify |
Identify |
|
Illuminance measurement |
|
Optional |
|
OTA upgrade |
|
Groups |
|
Parent topic:Light Level Sensor |
Device Structure
The following tsZLO_LightLevelSensorDevice structure is the shared structure for a Light Level Sensor device:
typedef struct
{
tsZCL_EndPointDefinition sEndPoint;
/* Cluster instances */
tsZLO_LightLevelSensorDeviceClusterInstances sClusterInstance;
/* Mandatory server clusters */
#if (defined CLD_BASIC) && (defined BASIC_SERVER)
/* Basic Cluster - Server */
tsCLD_Basic sBasicServerCluster;
#endif
#if (defined CLD_IDENTIFY) && (defined IDENTIFY_SERVER)
/* Identify Cluster - Server */
tsCLD_Identify sIdentifyServerCluster;
tsCLD_IdentifyCustomDataStructure
sIdentifyServerCustomDataStructure;
#endif
#if (defined CLD_ILLUMINANCE_LEVEL_SENSING) && (defined
ILLUMINANCE_LEVEL_SENSING_SERVER)
tsCLD_IlluminanceLevelSensing
sIlluminanceLevelSensingServerCluster;
#endif
/* Optional server clusters */
#if (defined CLD_POLL_CONTROL) && (defined POLL_CONTROL_SERVER)
tsCLD_PollControl sPollControlServerCluster;
tsCLD_PollControlCustomDataStructure
sPollControlServerCustomDataStructure;
#endif
/* Mandatory server clusters */
#if (defined CLD_IDENTIFY) && (defined IDENTIFY_CLIENT)
/* Identify Cluster - Client */
tsCLD_Identify sIdentifyClientCluster;
tsCLD_IdentifyCustomDataStructure
sIdentifyClientCustomDataStructure;
#endif
/* Recommended Optional client clusters */
#if (defined CLD_GROUPS) && (defined GROUPS_CLIENT)
/* Groups Cluster - Client */
tsCLD_Groups sGroupsClientCluster;
tsCLD_GroupsCustomDataStructure sGroupsClientCustomDataStructure;
#endif
#if (defined CLD_OTA) && (defined OTA_CLIENT)
tsCLD_AS_Ota sCLD_OTA;
tsOTA_Common sCLD_OTA_CustomDataStruct;
#endif
} tsZLO_LightLevelSensorDevice;
Parent topic:Light Level Sensor
Registration Function
The following eZLO_RegisterLightLevelSensorEndPoint() function is the endpoint registration function for a Light Level Sensor device.
teZCL_Status eZLO_RegisterLightLevelSensorEndPoint(
uint8 u8EndPointIdentifier,
tfpZCL_ZCLCallBackFunction cbCallBack,
tsZLO_LightLevelSensorDevice *psDeviceInfo);
Description
This function is used to register an endpoint which supports a Light Level Sensor device. The function must be called after eZCL_Initialise().
The specified identifier for the endpoint is a number in the range 1 to 240 (endpoint 0 is reserved for ZigBee use). Application endpoints are normally numbered consecutively starting at 1. The specified number must be less than or equal to the value of ZLO_NUMBER_OF_ENDPOINTS defined in the zcl_options.h file, which represents the highest endpoint number used for applications.
While invoking this function, specify a user-defined callback function, which is invoked when an event associated with the endpoint occurs. This callback function is defined according to the typedef:
typedef void( *tfpZCL_ZCLCallBackFunction)
(tsZCL_CallBackEvent *pCallBackEvent);
Also provide a pointer to a tsZLO_ColourControllerDevice structure, described in Section 3.16.2. This structure stores all variables relating to the color Controller device associated with the endpoint. The sEndPoint and sClusterInstance fields of this structure are set by this function and must not be directly written to by the application.
The function is called multiple times if more than one endpoint is being used - for example, if more than one Light Level Sensor device is housed in the same hardware, sharing the same module.
Parameters
u8EndPointIdentifier: Endpoint that is to be associated with the registered structure and callback function.
cbCallBack: Pointer to the function that is used to indicate events to the application for this endpoint.
psDeviceInfo: Pointer to the structure that acts as storage for all variables related to the device being registered on this endpoint (see Section 3.16.2). The
sEndPointandsClusterInstancefields are set by this register function for internal use and must not be written to by the application.
Returns
E_ZCL_SUCCESS
E_ZCL_FAIL
E_ZCL_ERR_PARAMETER_NULL
E_ZCL_ERR_PARAMETER_RANGE
E_ZCL_ERR_EP_RANGE
E_ZCL_ERR_CLUSTER_0
E_ZCL_ERR_CALLBACK_NULL
E_ZCL_ERR_CLUSTER_NULL
E_ZCL_ERR_SECURITY_RANGE
E_ZCL_ERR_CLUSTER_ID_RANGE
E_ZCL_ERR_MANUFACTURER_SPECIFIC
E_ZCL_ERR_ATTRIBUTE_TYPE_UNSUPPORTED
E_ZCL_ERR_ATTRIBUTE_ID_ORDER
E_ZCL_ERR_ATTRIBUTES_ACCESS
The above codes are described in the ZCL User Guide (JNUG3132).
Parent topic:Light Level Sensor
Parent topic:Lighting and Occupancy Device Types