‘Criticality Level’ Enumerations

The criticality levels that are available for an LCE are enumerated in the teSE_DRLCCriticalityLevels structure below:

typedef enum
{
    E_SE_DRLC_RESERVED_0_CRITICALITY = 0x00,
    E_SE_DRLC_GREEN_CRITICALITY,
    E_SE_DRLC_VOLUNTARY_1_CRITICALITY,
    E_SE_DRLC_VOLUNTARY_2_CRITICALITY,
    E_SE_DRLC_VOLUNTARY_3_CRITICALITY,
    E_SE_DRLC_VOLUNTARY_4_CRITICALITY,
    E_SE_DRLC_VOLUNTARY_5_CRITICALITY,
    E_SE_DRLC_EMERGENCY_CRITICALITY,
    E_SE_DRLC_PLANNED_OUTAGE_CRITICALITY,
    E_SE_DRLC_SERVICE_DISCONNECT_CRITICALITY,
    E_SE_DRLC_UTILITY_DEFINED_1_CRITICALITY,
    E_SE_DRLC_UTILITY_DEFINED_2_CRITICALITY,
    E_SE_DRLC_UTILITY_DEFINED_3_CRITICALITY,
    E_SE_DRLC_UTILITY_DEFINED_4_CRITICALITY,
    E_SE_DRLC_UTILITY_DEFINED_5_CRITICALITY,
    E_SE_DRLC_UTILITY_DEFINED_6_CRITICALITY,
    E_SE_DRLC_FIRST_RESERVED_CRITICALITY
} teSE_DRLCCriticalityLevels;

The above criticality levels are described in the table below.

Criticality Level Enumeration

Description

E_SE_DRLC_RESERVED_0_CRITICALITY

Reserved for future use

E_SE_DRLC_GREEN_CRITICALITY

Green: Indicates that there will be a significant contribution from non-green sources during the LCE - participation in the LCE is voluntary

E_SE_DRLC_VOLUNTARY_1_CRITICALITY

Voluntary 1-6: Represent increasing levels of load reduction as move through levels 1 to 6, as defined by the utility company - intended to be used in a sequence of LCEs to gradually reduce loads, where participation in the LCEs is voluntary

E_SE_DRLC_VOLUNTARY_2_CRITICALITY

E_SE_DRLC_VOLUNTARY_3_CRITICALITY

E_SE_DRLC_VOLUNTARY_4_CRITICALITY

E_SE_DRLC_VOLUNTARY_5_CRITICALITY

E_SE_DRLC_EMERGENCY_CRITICALITY

Emergency: Indicates that the LCE represents an emergency situation (normally demanding the termination of all non-essential loads, as defined by the utility company) - participation in the LCE is mandatory

E_SE_DRLC_PLANNED_OUTAGE_CRITICALITY

Planned Outage: Indicates that the LCE represents an intentional outage (normally demanding the termination of all non-essential loads, as defined by the utility company) - participation in the LCE is mandatory

E_SE_DRLC_SERVICE_DISCONNECT_CRITICALITY

Service Disconnect: Indicates that the LCE represents a service disconnection (normally demanding the termination of all non-essential loads, as defined by the utility company) - participation in the LCE is mandatory

E_SE_DRLC_UTILITY_DEFINED_1_CRITICALITY

Utility-defined 1-6: Criticality levels completely defined by the utility company - participation in the LCE is voluntary

E_SE_DRLC_UTILITY_DEFINED_2_CRITICALITY

E_SE_DRLC_UTILITY_DEFINED_3_CRITICALITY

E_SE_DRLC_UTILITY_DEFINED_4_CRITICALITY

E_SE_DRLC_UTILITY_DEFINED_5_CRITICALITY

E_SE_DRLC_UTILITY_DEFINED_6_CRITICALITY

E_SE_DRLC_FIRST_RESERVED_CRITICALITY

Reserved for future use

Parent topic:Enumerations