eSE_DRLCCreate

teZCL_Status eSE_DRLCCreate(
    bool_t bIsServer,
    uint8 u8NumberOfRecordEntries,
    uint8 *pu8AttributeControlBits,
    tsZCL_ClusterInstance *psClusterInstance,
    tsZCL_ClusterDefinition *psClusterDefinition,
    tsSE_DRLCCustomDataStructure
    *psCustomDataStructure,
    tsSE_DRLCLoadControlEventRecord
    *psDRLCLoadControlEventRecord,
    void *pvEndPointSharedStructPtr);

Description

This function creates an instance of the DRLC cluster on an endpoint. The cluster instance is created on the endpoint which is associated with the supplied tsZCL_ClusterInstance structure and can act as a server or a client, as specified.

The function should only be called when setting up a custom endpoint containing one or more selected clusters (rather than the whole set of clusters supported by a standard ZigBee device). This function creates a DRLC cluster instance on the endpoint, but instances of other clusters may also be created on the same endpoint by calling their corresponding creation functions. For more details of creating cluster instances on custom endpoints, refer to Appendix D.

Note: This function must not be called for an endpoint on which a standard ZigBee device (example, IPD) will be used. In this case, the device and its supported clusters must be registered on the endpoint using the relevant device registration function from those described in the ZigBee Devices User Guide (JNUG3131).

When used, this function must be the first DRLC cluster function called in the application, and must be called after the stack has been started and after the ZCL has been initialized.

The function requires an array to be declared for internal use, which contains one element (of type uint8) for each attribute of the cluster. The array length should therefore equate to the total number of attributes supported by the DRLC cluster.

The function initializes the array elements to zero.

Parameters

  • bIsServer: Type of cluster instance (server or client) to be created:

    • TRUE - server

    • FALSE - client

  • u8NumberOfRecordEntriesNumber of LCEs that can be stored in the LCE list, one of:

    • SE_DRLC_NUMBER_OF_SERVER_LOAD_CONTROL_ENTRIES

    • SE_DRLC_NUMBER_OF_CLIENT_LOAD_CONTROL_ENTRIES

  • pu8AttributeControlBitsPointer to an array of uint8 values, with one element for each attribute in the cluster (see above).

  • psClusterInstancePointer to structure containing information about the cluster instance to be created (see Section 6.1.16). This structure is updated by the function by initializing individual structure fields.

  • psClusterDefinitionPointer to structure indicating the type of cluster to be created (see Section 6.1.2). In this case, this structure must contain the details of the DRLC cluster. This parameter can refer to a pre-filled structure called sCLD_DRLC which is provided in the DRLC.h file.

  • psCustomDataStructurePointer to structure which contains custom data for the DRLC cluster. This structure is used for internal data storage. No knowledge of the fields of this structure is required.

  • psDRLCLoadControlEventRecord

  • Pointer to a structure in which an LCE is stored

  • pvEndPointSharedStructPtrPointer to the shared structure used for attribute storage. This parameter should be the address of the structure of type tsCLD_DRLC which defines the attributes of DRLC cluster. The function initializes the attributes with default values.

Returns

  • E_ZCL_SUCCESS

  • E_ZCL_FAIL

  • E_ZCL_ERR_PARAMETER_NULL

  • E_ZCL_ERR_INVALID_VALUE

Parent topic:Functions