Command Summary
The IAS ACE cluster includes a number of commands that can be sent by the application on the client or server. These commands are summarised below.
Table 50 lists the commands that can be issued on the client.
Table 51 lists the commands that can be issued on the server.
Functions are provided to send these commands - these functions are indicated in the descriptions below and detailed in Section 38.6.
IAS ACE Cluster Commands from Client to Server
Command |
Description and Function |
|---|---|
Arm |
Instructs the server to put all or certain enrolled zones into the ‘armed’ state or put all of them into the ‘disarmed’ state. |
Bypass |
Instructs the server to take one or more specified zones out of the system for the current activation (these zones are reinstated the next time the system is dis-armed and to exclude them again the next time the system is armed, the Bypass command must be re-sent before sending the Arm command). |
Emergency |
Instructs the server to put the alarm in the ‘Emergency’ state. |
Fire |
Instructs the server to put the alarm in the ‘Fire’ state. |
Panic |
Instructs the server to put the alarm in the ‘Panic’ state. |
Get Zone ID Map |
Requests the Zone IDs that have been allocated to zones. |
Get Zone Information |
Requests information on a specified zone. |
Get Panel Status |
Requests the current status of the (display) panel. |
Get Bypassed Zone List |
Requests a list of the currently bypassed zones. |
Get Zone Status |
Requests a list of either all zones with their status or those zones with a particular status (that is, all zones with the b16ZoneStatus attribute of the IAS Zone cluster having a certain value). eCLD_IASACE_GetZoneStatusSend() |
IAS ACE Cluster Commands from Server to Client
Command |
Description and Function |
|---|---|
Set Bypassed Zone List |
Informs the client which zones are currently bypassed and can be sent in response to a Bypassed Zone List command, Get eCLD_IASACE_SetBypassedZoneListSend() |
Zone Status Changed |
Informs the client that the status (value of the b16ZoneStatus attribute of the IAS Zone cluster) of a particular zone has changed. |
Panel Status Changed |
Informs the client that the status of the (display) panel has changed. eCLD_IASACE_PanelStatusChanged() |
Parent topic:IAS Ancillary Control Equipment Cluster