Compile-time options
To enable the IAS ACE cluster in the code to be built, it is necessary to add the following to the zcl_options.h file:
#define CLD_IASACE
In addition, to include the software for a cluster client or server or both, it is necessary to add one of the following to the same file:
#define IASACE_SERVER
#define IASACE_CLIENT
The IAS ACE cluster contains macros that may be specified at compile-time by adding one or more of the following lines to the zcl_options.h file.
Maximum Size of Zone Table
The maximum number of entries in a Zone table on the cluster server can be defined using the following line:
#define CLD_IASACE_ZONE_TABLE_SIZE n
where n is the desired maximum (e.g. 8).
Maximum Length of Arm/Disarm Code
The maximum length of string allowed for the arm/disarm code can be defined using the following line:
#define CLD_IASACE_MAX_LENGTH_ARM_DISARM_CODE n
where n is the desired maximum.
Maximum Length of Zone Label
The maximum length of string allowed for a zone name/label can be defined using the following line:
#define CLD_IASACE_MAX_LENGTH_ZONE_LABEL n
where n is the desired maximum.
Disable APS Acknowledgements for Bound Transmissions
APS acknowledgements for bound transmissions from this cluster can be disabled using the following line:
#define CLD_IASACE_BOUND_TX_WITH_APS_ACK_DISABLED
Cluster Revision
Add this line to define the value (n) of the Cluster Revision attribute:
#define CLD_IASACE_CLUSTER_REVISION <n>
The default value is 1, which corresponds to the revision of the cluster in the ZCL r6 specification (see Section 2.4).
Parent topic:IAS Ancillary Control Equipment Cluster