IAS WD Structure and Attribute
The structure definition for the IAS WD cluster is:
typedef struct
{
#ifdef IASWD_SERVER
zuint16 u16MaxDuration;
#endif
zuint16 u16ClusterRevision;
} tsCLD_IASWD;
where:
u``16MaxDurationis the maximum duration, in seconds, for which the alarm can be continuously active (for example, a siren sounded). The range of possible values is 0 to 65534 seconds and the default value is 240 seconds.u16ClusterRevisionis a mandatory attribute that specifies the revision of the cluster specification on which this cluster instance is based. The cluster specification in the ZCL r6 corresponds to a cluster revision of 1. The value is incremented by one for each subsequent revision of the cluster specification. This attribute is also described in Section 2.4.
Parent topic:IAS Warning Device Cluster