Auto-Enroll-Request
The Auto-Enroll-Request method of enrollment is described below:
After the IAS Zone device joins the network, the CIE device performs a service discovery.
If the CIE device determines that it wants to enroll the Zone device, it sends a
Write Attributecommand to the Zone device in order to write its IEEE/MAC address to the relevant attribute.The Zone device may optionally create a binding table entry for the CIE device and store the CIE device’s IEEE/MAC address there.
The Zone device sends a
Zone Enroll Requestcommand to the CIE device.The CIE device assigns a
Zone IDto the Zone device and sends aZone Enroll Responsecommand to it.The Zone device updates its attributes to stored the assigned Zone ID and update its zone state to ‘enrolled’.
Note: The above Auto-Enroll-Request process is similar to the Trip-to-Pair process (described in Section 37.3.2) except that user authorization for the enrollment of the Zone device is not required.
Parent topic:Enrollment