eCLD_IASZoneUpdateCIEAddress
teZCL_Status eCLD_IASZoneUpdateCIEAddress(
uint8 u8SourceEndPoint,
u64IEEEAddress u64CIEAddress);
Description
This function can be used on an IAS Zone cluster server to update the 64-bit IEEE/MAC address stored in the u64IASCIEAddress attribute. This is the address of the CIE device to which the local device should send commands and notifications.
Parameters
u8SourceEndPointId: Number of the endpoint on which the IAS Zone cluster resides
u64CIEAddress: IEEE/MAC address to be written to the attribute
Returns
E_ZCL_SUCCESS
E_ZCL_FAIL
Parent topic:Functions