eCLD_IASZoneUpdateZoneStatus
teZCL_Status eCLD_IASZoneUpdateZoneStatus(
uint8 u8SourceEndPoint,
uint16 u16StatusBitMask,
bool_t bStatusState);
Description
This function can be used on an IAS Zone cluster server to update the zone status bitmap stored in the b16ZoneStatus attribute, described in Section 37.2.
In one call to this function, one or more selected bits in the b16ZoneStatus attribute bitmap can be to set to ‘1’ or ‘0’. The affected bits must themselves be specified in a bitmap and the value to be set must also be specified.
If the server is enrolled with a client on a CIE device, the function sends a notification of this update to the client, in a Zone Status Change Notification. Before sending the notification and returning, the function invokes a user-defined callback function to allow the application to validate the status change.
Parameters
u8SourceEndPointId: Number of the endpoint on which the IAS Zone cluster resides
u16StatusBitMask: 16-bit bitmap indicating the bits of the
zb16ZoneStatusbitmap to be updated. There is a one-to-one correspondence between the bits of the two bitmaps and a bit should be set to ‘1’ if the corresponding attribute bit is to be updated. Enumerations are provided (which can be logical-ORed):
Bits |
Enumeration |
|---|---|
0 |
CLD_IASZONE_STATUS_MASK_ALARM1 |
1 |
CLD_IASZONE_STATUS_MASK_ALARM2 |
2 |
CLD_IASZONE_STATUS_MASK_TAMPER |
3 |
CLD_IASZONE_STATUS_MASK_BATTERY |
4 |
CLD_IASZONE_STATUS_MASK_SUPERVISION_REPORTS |
5 |
CLD_IASZONE_STATUS_MASK_RESTORE_REPORTS |
6 |
CLD_IASZONE_STATUS_MASK_TROUBLE |
7 |
CLD_IASZONE_STATUS_MASK_AC_MAINS |
8 |
CLD_IASZONE_STATUS_MASK_TEST |
9 |
CLD_IASZONE_STATUS_MASK_BATTERY_DEFECT |
10-15 |
Reserved |
bStatusState: Boolean indicating the value to which the attribute bits to be updated must be set - enumerations are provided:
CLD_IASZONE_STATUS_MASK_SET (1)CLD_IASZONE_STATUS_MASK_RESET (0)
Returns
E_ZCL_SUCCESS
E_ZCL_FAIL
Parent topic:Functions