Trip-to-Pair
The Trip-to-Pair method of enrollment is described below:
After the IAS Zone device joins the network, the CIE device performs a service discovery.
If the CIE device determines that it wants to enroll the Zone device, it sends a Write Attribute command to the Zone device in order to write its IEEE/MAC address to the relevant attribute.
The Zone device may optionally create a binding table entry for the CIE device and store the CIE device’s IEEE/MAC address there.
The Zone device waits for the authorization of the enrollment via a user input (for example, a button-press) and, on this input, sends a Zone Enroll Request command to the CIE device.
The CIE device assigns a Zone ID to the Zone device and sends a Zone Enroll Response command to it.
The Zone device updates its attributes to stored the assigned Zone ID and update its zone state to ‘enrolled’.
Parent topic:Enrollment