eSE_SMCreate
teZCL_Status eSE_SMCreate(
uint8 u8Endpoint,
bool_t bIsServer,
uint8 *pu8AttributeControlBits,
tsZCL_ClusterInstance *psClusterInstance,
tsZCL_ClusterDefinition *psClusterDefinition,
tsSM_CustomStruct *psCustomDataStruct,
void *pvEndPointSharedStructPtr);
Description
This function creates an instance of the Simple Metering cluster on an endpoint. The cluster instance is created on the endpoint which is associated with the supplied tsZCL_ClusterInstance structure and can act as a server or a client, as specified.
The function should only be called when setting up a custom endpoint containing one or more selected clusters (rather than the whole set of clusters supported by a standard ZigBee device). This function will create a Simple Metering cluster instance on the endpoint, but instances of other clusters may also be created on the same endpoint by calling their corresponding creation functions. For more details of creating cluster instances on custom endpoints, refer to Appendix D.
Note: This function must not be called for an endpoint on which a standard ZigBee device (for example, an IPD) is used. In this case, the device and its supported clusters must be registered on the endpoint using the relevant device registration function from those described in the ZigBee Devices User Guide (JNUG3131).
When used, this function must be the first Simple Metering cluster function called in the application, and must be called after the stack has been started and after the ZCL has been initialized.
The function requires an array to be declared for internal use, which contains one element (of type uint8) for each attribute of the cluster. The array length should therefore equate be the total number of attributes supported by the Simple Metering cluster, which can be obtained by using the macro SM_NUM_OF_ATTRIBUTES.
The array declaration should be as follows:
uint8 au8AppSMClusterAttributeControlBits[SM_NUM_OF_ATTRIBUTES];
The function initializes the array elements to zero.
Parameters
u8Endpoint: Number of local endpoint on which the cluster instance is to be created, in the range 1 to 240.
bIsServer : Type of cluster instance (server or client) to be created:
: TRUE - server
: FALSE - client
pu8AttributeControlBits: Pointer to an array of uint8 values, with one element for each attribute in the cluster (see above).
psClusterInstance: Pointer to structure containing information about the cluster instance to be created (see Section 6.1.16). This structure is updated by the function by initialising individual structure fields.
psClusterDefinition: Pointer to structure indicating the type of cluster to be created (see Section 6.1.2). In this case, this structure must contain the details of the Simple Metering cluster. This parameter can refer to a pre-filled structure called
sCLD_SimpleMeteringwhich is provided in the SimpleMetering.h file.psCustomDataStructure: Pointer to structure which contains custom data for the Simple Metering cluster. This structure is used for internal data storage and also contains data relating to a received command/message. No knowledge of the fields of this structure is required.
pvEndPointSharedStructPtr: Pointer to the shared structure used for attribute storage. This parameter should be the address of the structure of type
tsCLD_SimpleMeteringwhich defines the attributes of Simple Metering cluster. The function will initialize the attributes with default values.
Returns
E_ZCL_SUCCESS
E_ZCL_FAIL
E_ZCL_ERR_PARAMETER_NULL
E_ZCL_ERR_INVALID_VALUE
Parent topic:Functions